REGEN.POWER

Description

This parameter reads regen resistor's calculated power, which is determined as follows:

(V2 / R) * DutyCycle

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

Watt

Range

N/A

Default Value

N/A

Data Type

Integer

See Also

N/A

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

REGEN.POWER

3007h

02h

Unsigned32

-

-

Read only

Yes

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

REGEN.POWER

2400

960

Unsigned32

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

REGEN.POWER

2400

Unsigned32

Read Only

-